Even the most efficient machine needs first-class clamping systems for fast, flexible and high-precision component machining. Mack Alusysteme plays it safe with the VERO‑S modular workholding system from SCHUNK. Pallet automation fires up the turbo for optimal machine utilization, and takes machining precision to a new level.

At Mack Alusysteme, precision is down to a hundredth. Production Manager Dominik Isele puts it in a nutshell: “Where others stop, we start.” A promise that is appreciated by customers from the aerospace, railroad, electronics, automotive, and general engineering industries. The prerequisite for precision manufacturing made in Klettau, Baden-Württemberg, is a state-of-the-art suite of machinery. For some time now, this has also included the five-axis milling center DMU 95 monoblock with a PH Cell 300 pallet automation system. “The system is a top performer,” emphasizes Isele. The VERO‑S quick-change pallet system from SCHUNK is at the heart of fully automated component machining. It serves as a pallet changing unit, a robot coupling, and for workpiece direct clamping and thanks to these flexible functionalities cannot only handle several tasks but also cover different components with just one device.
The spindle runs 24/7
Machining on the machine takes some time due to the complexity of the components. It was therefore important to Isele to provide a stock of clamped parts of prefabricating blanks. The machine can then process this stock successively and automatically. “Our aim was to maximize the spindle running time and to fully automate the pallet infeed and outfeed,” confirms Isele. Mack has achieved this goal with the VERO‑S clamping system from SCHUNK. The spindle is in operation 24/7 thanks to the pre-prepared pallets in the pallet station, and the fully automatic supply and removal of pallets.
“Our aim was to maximize the spindle running time, and to fully automate the pallet infeed and outfeed.”
Dominik Isele, Production Manager Mack Alusysteme

Access from five sides
However, speed and efficiency are not the only requirements Isele has for the new machine. “We’ve got aluminum profiles that we have to machine on five sides. Good accessibility was therefore important to us,” he says. The direct workpiece clamping system WDM-5X from the VERO‑S modular system of SCHUNK completely convinced him with its optimal workpiece accessibility during five-sided machining. The pillar clamping principle of the WDM-5X enables penetrations across the entire workpiece – naturally without an interfering contour.
The base modules WDM-5X serve as a basis on the pallet. Different processing heights can be implemented with combinable stacking modules in different heights. The clamping pin connects the workpiece to the clamping pillar. Mack uses the dove tail version of the clamping pin. “It gives us several advantages,” enthuses Isele. The clamping pin allows direct clamping of flat workpieces, which have a clamping depth of just 3.5 millimeters. This opens up new possibilities for processing thin workpieces, mold halves or free-form parts. Its trapezoidal shape additionally increases the contact surface through which clamping forces are absorbed. In turn, this enables a lower clamping depth for a force-fit connection. “This saves us raw material and we didn’t have to make any changes to the material purchase order,” says Isele happily.

Get started automatically well prepared
The pallets with the WDM-5X modules and the blanks are set up in a separate, ergonomically designed set-up station. Manual set-up is so simple that even unskilled workers can do it. The pallet with the clamped workpieces is then picked up by the robot, stored in the pallet station and fed to the machine when requested. The robot coupling VERO‑S NSR 160 is the interface between the workpiece pallet and the robot. The high pull-down force on the robot-side clamping pin has such a high holding force that even heavy pallets can be handled reliably. Production Manager Dominik Isele is completely satisfied with the clamping system: “Everything fits together, finding the solution with SCHUNK, the implementation of the design, and the flexible clamping system itself. This is a true all-round carefree package for us and is done simply and smartly.”

1.
Dove tail pin
2.
Inserting the dove tail pin into the workpiece


3.
Direct clamping without interfering contours with WDM-5X
Our customer:
Mack Alusysteme
Mack Alusysteme is a contract manufacturer for customers in the aerospace, construction, electrical engineering, automotive and general engineering industries. A good 100 employees work in the milling, assembly, welding, and ladder and railing construction departments at the plant in Klettgau in the southern Black Forest.
The third-generation, owner-managed family business exclusively processes aluminum – from sample production to series production. Mack meets the high demands of its customers and ensures maximum precision through a quality management system for each individual part.
Learn more:
The spindle never stops running