The company Neher is excited about its use of the VERO‑S NSE-HT mini 88–20 clamping system from SCHUNK in the additive manufacturing of metal tools. The completely sealed clamping module can withstand heat, dust and immersion baths. It is therefore suitable for particularly demanding applications – including powder bed 3D printing (SLM) – because here it offers absolute reliability, high flexibility and short set-up times.
SCHUNK modules are installed at a number of production locations at Neher. For the production of customized special tools for the automotive industry, the company in Ostrach-Einhart uses various toolholders, chuck jaws, lathe chucks and vises from SCHUNK.
As a top performer, Neher needs reliable production components to meet the high customer requirements for both tool clamping and workpiece clamping. “We need top quality in any case,” says Tobias Niess, Developer at Neher. All the more so when it comes to particularly demanding parts production, such as the additive manufacturing of highly specific tools made of metal. This is where the VERO‑S NSE-HT mini 88–20 quick-change pallet system comes into focus. The clamping system for use in high-temperature applications remains unaffected by the finest dusts, abrasive materials and even continuous immersion baths.
There are challenges beyond what clamping systems need to withstand in everyday, conventional machining processes. “We can’t imagine our production processes without this quick-change pallet system,” says Tobias Niess. And he knows exactly what he’s talking about.
Quick-change pallet system as the basis for precision
He and his team oversee 3D metal printing at the company. For this purpose, the company purchased the modern Lasertec 30 Dual SLM from DMG Mori for generative manufacturing by selective laser melting (SLM). This “3D printer” can be used to generatively manufacture highly complex components with differentiated functional integration in a powder bed heated up to 200 degrees Celsius. This so-called hybrid printing process, melting workpieces onto prefabricated components, is also achieved at Neher. In this process, geometrically simple workpiece components are manufactured conventionally, and the complex geometries are then additively “printed” onto the hybrid blank. For this purpose, the clamping pins of the quick-change pallet system are mounted directly on the hybrid blank.
This approach utilizes the advantages of both processes and significantly reduces manufacturing costs. The runtime of the 3D printer is shortened, meaning it can move on to the next job faster.
A prerequisite for the precise and efficient production of these kinds of workpieces is the absolutely precise clamping of the substrate plate on which the product is additively built in the machine room. This is where the VERO‑S NSE-HT mini 88–20, which SCHUNK designed and laid out specifically for applications in 3D metal printing, stands out.
Heat resistant and perfect for 3D metal printing
“This clamping module is special,” says Developer Benjamin Hirz. “While conventional quick-change pallet systems can be used up to 60 degrees Celsius, this clamping system withstands the high temperatures of the steel powder melting process.” “Without the VERO‑S NSE-HT mini 88–20, we would not be able to implement the thermally demanding manufacturing process. It always reliably guarantees us the fixed position on the machine table side,” explains Tobias Niess.
“We can't imagine our production processes without this quick-change pallet system!”
Tobias Niess,
Developer at the Neher Group
At Neher, four VERO‑S NSE-HT mini 88–20 modules are used, as well as a VERO‑S NE-HT mini 36 quick-change pallet unit in the center. The quick-change pallet unit defines the thermal zero point for large substrate plates via a centric clamping pin. The clamping itself takes place simultaneously via the remaining four clamping pins. An integrated spring assembly secures the clamping permanently and is self-locking– air is only required for the opening process.
Sealing concept keeps out dust and abrasive materials
The second major challenge for the clamping system is that it is permanently exposed to the highly abrasive materials. But the SCHUNK sealing concept makes it possible to resist the finest metal dusts that penetrate even the tiniest crevices.
“Our sealing concept is so reliable that the clamping system is even suitable for immersion baths,” confirms Benjamin Hirz. “Under all of these environmental conditions, a permanently high force is maintained on the clamping slide, which ensures absolute process reliability. Even if fine metal powder gets into the cutting area, the clamping slides do not get blocked. The module clamps reliably.”
Long life span
One single VERO‑S NSE-HT mini 88–20 has been running on the 3D metal printer at Neher for three years. “Absolutely reliable and trouble-free and one hundred percent precise,” Tobias Niess emphasizes. Despite the long machining times of seven to ten hours in 3D metal production, SCHUNK states that the service life of a quick-change pallet system used in this way is approximately ten years.
Special tools manufacturer
Among other things, Neher manufactures standard and special tools as well as components for a wide variety of applications, including powertrain modules for the automotive industry.
In addition to modern CNC-controlled turning and milling machining centers, several 3D metal printers as well as corresponding measuring technology have been in use for several years, which is why the company can produce a wide variety of customized components in lightweight structure with functional integration.
The one-man operation founded in Ostrach in 1990 as Neher Diamantwerkzeuge has developed into a state-of-the-art company that currently has around one hundred employees. Since June 2021, Neher has expanded its business field to include fixture construction, jig construction and measurement technology.
Neher Group
www.neher-group.com