Mr. Rombach, why did you switch from the proven SRU-plus swivel module to the SRM unit?
In our flexible cells, we handle very small as well as relatively large parts. One single automation solution needs to be able to cover this performance spectrum on one machine. We had designed the SRU-plus ourselves, but it was simply too small and could not provide the necessary power. But with the limited installation space, we could not install a larger unit.
Then came the solution that saved the day when SCHUNK recommended the newly dimensioned SRM to us. This swivel module is now available in all step sizes, meaning we have been able to access the size that suits us best.
Despite the relatively small installation space, the SRM provides higher maximum moments and better damping, and runs with absolute stability.
“Despite the relatively small installation space, the SRM provides higher maximum moments and runs with absolute stability.”
Marco Rombach
Do you also use the SRM swivel unit in other applications?
The SRM has come into use throughout our company ever since then, because it enables a downward leap in size with greater power density at the same time. Since our core concept is to build compact cells that are also easy to integrate into the customer’s space, installation space is always an issue for us. We always need full performance in the smallest possible space. That’s why the SRM has come at just the right time for us.
It is noticeable that several SCHUNK modules are used in each system, both grippers in all versions and swivel units. Are there no alternatives for you?
Perhaps there are alternatives. But what we need is absolute reliability, and we find that with SCHUNK components. Our customers depend on reliability. Their systems run 24/7 all year round. Maximum throughput, no downtime and high flexibility are the
specifications.
Reliability is at the top of the list, and we don’t allow ourselves any experiments here, because the customer needs the best possible delivery performance. And we can only achieve this with top quality, which is why we rely on SCHUNK.
Black Forest Smart Automation
www.bfsa-automation.com
Source of innovation in the Black Forest
Black Forest Smart Automation – BFSA – is an automation specialist based in Löffingen, Germany. The core of the solutions is the “smart cell”, which can be equipped in a customer-specific and modular way depending on the application. In compact Euro pallet size, it can be integrated into existing processes and expanded as required.
This results in flexible and modular cells for palletizing, stacking, cleaning, labeling, deburring or handling in different industries.
The SRM rotary module: versatility in modules.
The swivel unit SRM 25 offers BFSA maximum flexibility.
BFSA has integrated the SRM 25 into a customized automation cell and supplemented it with a variety of SCHUNK grippers. In this cell, pre-turned parts are fed to a knurling machine. The SRM swivel unit then performs a crucial function in the cell: when the knurled component is removed from the machine, it is pointing downward; for placement on the conveyor belt, the swivel unit rotates it upwards by 180 degrees.
The SRM 25 swivel unit in use at BFSA:
Due to the tight installation space at this pick-and-place station, the focus of BFSA for the cell design was on performance and compactness. Since SCHUNK has been offering the SRM pneumatic swivel module in all sizes as of this year, BFSA can use it instead of the SRU-plus module it originally used.
The greater torque of the SRM module and the high energy absorption of the shock absorbers mean that the components are set down precisely and gently. “We get higher performance within the same installation space, and we can easily handle swiveling the eccentric load beyond the twelve o’clock point,” confirms Rudolf Martin, Design and Manufacturing Manager at BFSA.
BFSA also relies on SRM modules in a labeling cell. Here, turned parts are guided by SCHUNK SRM 16 swivel modules in perfect interaction with the PGN-plus‑P parallel grippers and the PZN-plus three-jaw gripper precisely through the labeling process and on to the next machining step.
Turning components by 180° with SCHUNK SRM
Product information:
schunk.com/SRM