Battery cell manufacturing must balance extreme cleanliness, maximum precision, and increasing production rates – only manufacturers that master all three can ensure quality and cost-effectiveness.
Clean
In battery cell manufacturing, even the tiniest impurities can determine whether a cell is a reject or functions properly. Microscopic particles can damage sensitive separators or trigger chemical reactions. Moisture compromises material stability. At the same time, processes involve ultra-thin foils and sensitive coatings that are extremely susceptible to environmental influences. The solution lies in consistently controlled production environments: cleanrooms and dry rooms with minimal particle and moisture loads, combined with reliable, low-emission automation, provide the basis for consistent quality and reliably functioning cells. SCHUNK products for battery cell manufacturing feature high-quality anodized finishes and are certified for cleanrooms and dry rooms. Special lubricants are lithium-free and retain their properties even under extremely dry conditions.
Precise
Even the slightest deviations in positioning lead to electrical imbalances and mechanical stresses in cell manufacturing, resulting in rejects. Tolerances in the micrometer range are critical when stacking anodes, cathodes, and separators, or when cutting extremely thin electrode foils. At the same time, delicate materials are highly sensitive to even the slightest forces or vibrations. End-to-end precision is therefore essential: accurate guidance and positioning, reproducible motion sequences, and continuous monitoring ensure the necessary repeat accuracy along the entire process chain. SCHUNK grippers, for example, are designed to move components safely and position them precisely in line with requirements such as maximum surface pressure or a defined gripping range.
Quick
The growing demand for battery cells is increasing the pressure on production speed and costs. High production volumes require extremely short cycle times – for example, when stacking, with each layer taking just a few tenths of a second. At the same time, speed must not come at the expense of quality, as errors have an immediate economic impact.
The key is the interplay between speed and stability: highly dynamic, automated processes, short setup times and downtimes, and end-to-end process control enable high output while maintaining consistent quality. SCHUNK systems increase cycle speed through features such as parallel processing lines or extremely fast tool changes, for example in slitting.
SCHUNK solutions
for the battery production process

Mixing
Homogeneous mixing of active materials and binders

Coating
Coating the electrode foils with active material

Drying
Drying the coated electrodes under controlled conditions

Calendering
Compressing the electrodes to achieve specific material properties

Slitting
Cutting the electrode strips to the exact width
Precision through hydraulic expansion technology
In slitting, the key is to achieve consistently precise cut quality with high machine availability. Even the slightest deviations have a direct impact on electrode quality. At the same time, knife changes must be performed quickly to minimize downtimes. Hydraulic expansion technology enables low-vibration clamping of the cutting knives, ensuring stable processes, cleanly cut edges, and high efficiency during operation.

Hydraulic
expansion arbor

Vacuum drying
Removal of residual moisture under vacuum conditions

Stacking
Stacking the anode, cathode, and separator in layers
Precise handling of electrodes for pouch and prismatic cells
In stacking, positioning accuracy and cycle time determine the quality of the cell stacks. Even minimal misalignments can lead to defective layer structures and result in rejects. Electrode layers can be positioned precisely through carefully controlled movements and synchronized sequences. Process steps conducted in parallel further increase speed and improve yield.

Stacking
unit

Packaging
Inserting the cell stack into the housing
Safe transportation without displacement
After stacking, delicate cell stacks must be transported reliably and with full process control. Even a slight misalignment of the layers will impair the cell’s function. Stable mounting combined with gentle handling is therefore essential. Customized gripping and holding concepts reliably secure the stack, minimize mechanical stresses, and ensure consistently high quality throughout the process chain.

Handling
unit

Filling
Filling the cell with electrolyte

Formatting
Initial charging to activate the electrochemical processes
Efficient loading and unloading of battery cells
During the formatting and aging process steps, the battery cells’ chemical function is activated. Handling large volumes of cells in short cycles places high demands on efficiency and process reliability. What is needed are flexible, automated processes that enable a rapid flow of materials while ensuring that the sensitive cells are handled with care.

Multiple
gripper unit

Degassing
Removing gases from the cell

Aging
Stabilizing cell chemistry through controlled storage
Efficient loading and unloading of battery cells
During the formatting and aging process steps, the battery cells’ chemical function is activated. Handling large volumes of cells in short cycles places high demands on efficiency and process reliability. What is needed are flexible, automated processes that enable a rapid flow of materials while ensuring that the sensitive cells are handled with care.

Multiple
gripper unit

Testing
Testing performance, safety, and quality